Jump to content
OMRON Forums

cmoncsko

Members
  • Posts

    3
  • Joined

  • Last visited

cmoncsko's Achievements

Newbie

Newbie (1/14)

  • Week One Done
  • One Month Later
  • One Year In

Recent Badges

0

Reputation

  1. No problem with the thread-jacking. I have been able to fix the problem by adding in the addins manually. I too find both "PowerPmacSuite" and "Power PMAC Suite" installed in "My Documents". This seems unusual, but I left it alone.
  2. The problem has gone away overnight. I have not touched the PMAC or PC since I posted yesterday and this morning it syncs to the database just fine. The PC hasn't rebooted, nor is it connected to the internet. New problem: All of the Add-Ins are now missing. If I select them in the menu, a message tells me that it cannot be located and asks me if I would like to remove it from the menu. I tried both the repair and the modify features of the PMAC Suite installer to try and re-install the addins, but it has not solved the problem. Are these issues related?
  3. I too am having this issue. I am running it on the same OS as Artag (32-bit XP SP3) with the same version of the IDE (Feb 2011) and I receive the "database sync function failed!" error and the motor setup runs into many problems. I have installed it as a user with admin rights, and I have also tried installing it as the Administrator user. Nothing is on a network, the whole install is local and in the default directories.
×
×
  • Create New...