cmoncsko
-
Posts
3 -
Joined
-
Last visited
Content Type
Profiles
Forums
Events
Downloads
Posts posted by cmoncsko
-
-
The problem has gone away overnight. I have not touched the PMAC or PC since I posted yesterday and this morning it syncs to the database just fine. The PC hasn't rebooted, nor is it connected to the internet. New problem: All of the Add-Ins are now missing. If I select them in the menu, a message tells me that it cannot be located and asks me if I would like to remove it from the menu. I tried both the repair and the modify features of the PMAC Suite installer to try and re-install the addins, but it has not solved the problem. Are these issues related?
-
I too am having this issue. I am running it on the same OS as Artag (32-bit XP SP3) with the same version of the IDE (Feb 2011) and I receive the "database sync function failed!" error and the motor setup runs into many problems. I have installed it as a user with admin rights, and I have also tried installing it as the Administrator user. Nothing is on a network, the whole install is local and in the default directories.
Database sync function failed
in Power PMAC
Posted