AhmetNuri
-
Posts
5 -
Joined
-
Last visited
Content Type
Profiles
Forums
Events
Downloads
Posts posted by AhmetNuri
-
-
you can wach the video for our servo motor.
http://www.2shared.com/video/hsRknapd/delta_tau_tecoservo.html
the firest step i use the mpg for motor control. then ı use jog in the video. My old servo motor 1000 rpm and has 5000 ppr encoder. My new servo motor (teko 1 kw with E series drive) 2000 rpm and 2500 ppr .
and my old i parameters are
i230=5719
i231=5747
i232=6441
i233=16611
i234=1
i235=82902
how can i calculate new i parameter for new drive?
-
Yes , I have I230, 231,232,232,234,235 paramters.
This would be best handled as at Technical Support issue.
Was this motor OK before changes to the noted I-variables?
Please respond to smilici@deltatau.com.
-
I see some parameters for motor settings
Is any one can explain me what is
I230
I231
I232
I233
I234
parameters on the adv 400 ?
thanks.
-
Hi, I have Adv 400 cnc unit. We have a servo motor problem. And we change the servo motor and drive. We use analog mod. I change I230 paramater on the terminal.
I can control motor with mpg. it seems normaly. I use Jog mod f5 or f6
motor start work but when the motor stoped 1 or 1/2 cycle turns in the opposite direction. why?
the problem is 2. motor.
you can see the motor 2 setting from pictures
adv 400 and serial connection
in Pre-Turbo PMAC
Posted
I think I need auto tuninig for my servo drive with adv 400.
I read form the adv 400 book, auto tunining need serial connection.
I install pmac suit 32 bit.
but there is no serial connection settings. there is only ethernet settings.
How can I connect adv 400 with pmac suit on seril connection=?