KiraYamato
Members-
Posts
17 -
Joined
-
Last visited
Content Type
Profiles
Forums
Events
Downloads
Everything posted by KiraYamato
-
hi, everyone i meet some problems when i use turbo pmac 2 to tune the pid parameter of an axes the motor i used pull via a screw I set kd=0 and a proper kp and ki and it seems that a step folloing is acceptable but the command velocity oscillated during a sine wave following the period of the oscillation and following error appears to coincide but i do not think that is a reasonable answer can any one spare me a help? 3q
-
Hello, every one I bought a ACC 1P module for my Turbo PAMC 2 Clipper I insert it on Turbo PAMC 2 Clipper the LED D3 turns red and sparkles I found that there is no Connector for the power supply, And I found that it seems to lost a chip on the back side of ACC 1P Is all of your the same?
-
thank you, mbalentine but the user manual said that I should disable the OT limit so as to use it as a normal trigger for a trigger move——home search, for example. Here are the codes I found, and the only difference is that I set I124 $920001 instead of $20000. P.S.: You said that :the Home function is reading the input as always true (no overtravel fault) & homing to the marker. Your graph indicates this. would you spare me a moment and explain more about that? ;*********** Motion Program Set-up Variables (to be saved) ************* CLOSE I123=-10 ; Home speed 10 cts/msec negative I124=$000000 ; PMAC-style flags, normal mode I125=$78000 ; Use Servo IC 0 Channel 1 flags for Motor 1 I126=32000 ; Home offset of +2000 counts ; (enough to take you out of the limit) I7102=3 ; Capture on rising flag and rising index I7103=2 ; Use +LIM1 as flag (negative end switch) ;*********** Motion program to execute routine ********************* OPEN PROG 101 CLEAR I124=$20000 ; Disable +/-LIM as limits HOME1 ; Home #1 into limit and offset out of it I124=$0 ; Re-enable +/-LIM as limits CLOSE ; End of program
-
Sir: Thank you for your attention. I connected as the manual shows. I set the M121:->X:$078000,17 And when I turned the switch, I saw that M121 chaged, but the flag monitor the state for PLIM hardward did not change and my setting for the variable is almost the same as the example user manual gives: ;*********** Motion Program Set-up Variables (to be saved) ************* CLOSE I123=-10 ; Home speed 10 cts/msec negative I124=$920001 ; PMAC-style flags, normal mode I125=$78000 ; Use Servo IC 0 Channel 1 flags for Motor 1 I126=32000 ; Home offset of +2000 counts ; (enough to take you out of the limit) I7012=3 ; Capture on rising flag and rising index I7013=2 ; Use +LIM1 as flag (negative end switch) and I use the on-line command to make the axis 1 home, but the axis showed that it complete home search while I did not turned the passive switch..... here is the position-time curve I got during the "homing" process: would you please give me some advice? Thank you very much~
-
Hi, everyone~ I need to connect the limit and home signal to my Turbo PMAC2 Clipper now. I read in the HRM that : I use a 34 pin passive Flat Cable commutator for the JMACH2 prot. So if I use the positive limit for axis 1, I just connnect pin 1 to a +5V power and pin 7 to a switch linked to the ground of the +5V power? But I can not see the text "soft or hardware limit" in the flag monitor change its color when I turned on and off the switch. What should I do? And what shall I do with pin 2(GND)? No connection? Thank you for your attention~
-
Blend under LINEAR mode when doing circular interpolation
KiraYamato replied to KiraYamato's topic in Turbo PMAC
Sir: thank you for your attention, but I really made no change else, and this time, it works successfully. Maybe I should change it back and see the difference. -
Blend under LINEAR mode when doing circular interpolation
KiraYamato replied to KiraYamato's topic in Turbo PMAC
The problem was solved, by moving the TM(P6) command It seems that I can not set the motion time in dynamic...... -
Blend under LINEAR mode when doing circular interpolation
KiraYamato replied to KiraYamato's topic in Turbo PMAC
Thank you ,sir I will try it~ Hope I can get a good result~ -
Blend under LINEAR mode when doing circular interpolation
KiraYamato replied to KiraYamato's topic in Turbo PMAC
Dear Sina: Thank you for your instruction. I just want to use the circular interpolation as a test fot the effect. I have a spatial curve to be followed, and I can generate the position and velocity commands for each axis. Then I should decide what kind of move modes should I use to give the commands. I tried the PVT command, but I got a peak in the velocity curve, which would enlarge the position error, so I want to see how about the LINEAR mode. -
Hello, everyone I am doing a circular interpolation under LINEAR mode I divide the radius angle by N so I have a constant move segment time then I compute each point on the circle and give them to the X and Y axis I read in the user manual that: PMAC will blend between the segment so if N is large enough the velocity of each axis will change smoothly but I did not get the expected result the shape of axis velocity looks like many peaks can you tell me how should I set PMAC to make the move blend? Here are my motion program: *********************************** &1 CLOSE UNDEFINE ALL #1->X #2->Y ;****** Motion Program Text ******* OPEN PROG 1 CLEAR abs P1=2000 ;radius P2=1000 ;divide central angle by N P3=3.1415926 ;Pi P4=0.32*P3 ;angular speed P5=1000*2*P3/P4 ;total move time P6=P5/P2 ; time between the interpolation points P11=0 ;loop counts LINEAR TM 100 X 0 Y 0 DWELL 500 While (P11 < P2+1) P21=2*P3*P11/P2 ;central angle P22=P1*(1-cos(P21*180/p3)); P23=P1*(sin(P21*180/p3)); P24=P4*P1*sin(P21*180/p3); P25=P4*P1*cos(P21*180/p3); TM(P6) X (P22) Y (P23) P11=P11+1 EndWhile CLOSE
-
Sina: Thank you for your edification. I found an easy example about kinematic program, and it works. And I followed your instruction and I can run the program given in the user manual. Now I will try to modify the code so that it will our virtual equipment, and my friend is dealing with the downloading of the program. Thanks again~
-
Hello, everyone I am trying to use Turbo PMAC 2 Clipper to control the servo motors in a robot system, I find the the example in Turbo PMAC USER MANUAL from page 261 to 266, and I get the codes. Now my question comes: How to deal with these code? Should I piece them together as a *.pmc file and download it directly? Or should I down load it separately,just like the *.h file and *.cpp? And where should I write my codes for motion program ? I attach the codes in the end Thank you for your attention~ ;---------------------------------------------------[/size][/font] ; Setup for program I15=0 ; Trig calculations in degrees &1 ; Address CS 1 M145->Y:$0000C0,10,1 ; Motor 1 home complete bit M245->Y:$000140,10,1 ; Motor 2 home complete bit M5182->Y:$00203F,22,1 ; CS 1 run-time error bit Q91=400 ; L1 Q92=300 ; L2 Q93=1000 ; Counts per degree for A and B ; Forward-kinematic program buffer for repeated execution &1 OPEN FORWARD ; Forward kinematics for CS 1 CLEAR ; Erase existing contents IF (M145=1 AND M245=1) ; Properly position referenced? Q7=Q91*COS(P1/Q93)+Q92*COS((P1+P2)/Q93) ; X position Q8=Q91*SIN(P1/Q93)+Q92*SIN((P1+P2)/Q93) ; Y position ELSE ; Not valid; halt operation M5182=1 ; Set run-time error bit ENDIF CLOSE ; M-variable definitions for actual position registers M162->D:$8B ; Motor 1 actual position M262->D:$10B ; Motor 2 actual position ; Forward-kinematic PLC program buffer for position reporting OPEN PLC 10 ; Forward kinematics for CS 1 CLEAR ; Erase existing contents P51=M162/(I108*32*Q93) ; Actual A position (deg) P52=M262/(I208*32*Q93) ; Actual B position (deg) Q27=Q91*COS(P51)+Q92*COS(P51+P52) ; Actual X position Q28=Q91*SIN(P51)+Q92*SIN(P51+P52) ; Actual Y position CLOSE ; Setup for program &1 #1->I ; Motor 1 assigned to inverse kinematic axis in CS 1 #2->I ; Motor 2 assigned to inverse kinematic axis in CS 1 M5182->Y:$00203F,22,1 ; CS 1 run-time error bit ; Pre-compute additional system constants Q94=Q91*Q91+Q92*Q92 ; L1^2 + L2^2 Q95=2*Q91*Q92 ; 2*L1*L2 Q96=Q91*Q91-Q92*Q92 ; L1^2 – L2^2 ; Inverse-kinematic algorithm to be executed repeatedly &1 OPEN INVERSE ; Inverse kinematics for CS 1 CLEAR ; Erase existing contents Q20=Q7*Q7+Q8*Q8 ; X^2+Y^2 Q21=(Q20-Q94)/Q95 ; cos(B) IF (ABS(Q21)<0.9998) ; Valid solution w/ 1 deg margin? Q22=ACOS(Q21) ; B (deg) Q0=Q7 ; X into cos argument for ATAN2 Q23=ATAN2(Q8) ; A+C = ATAN2(Y,X) Q24=ACOS((Q20+Q96)/(2*Q91*SQRT(Q20))) ; C (deg) Q25=Q23-Q24 ; A (deg) P1=Q25*Q93 ; Motor 1 = 1000A P2=Q22*Q93 ; Motor 2 = 1000B ELSE ; Not valid, halt operation M5182=1 ; Set run-time error bit ENDIF CLOSE &1 OPEN INVERSE CLEAR {Position calculations from above} IF (Q10=1) ; PVT mode? Q26=SIN(Q25) ; sin(B) IF (Q26>0.0175) ; Not near singularity? Q27=Q91*Q92*Q26 ; L1*L2*sinB Q28=COS(Q25+Q22) ; cos(A+B) Q29=SIN(Q25+Q22) ; sin(A+B) Q30=(Q92*Q28*Q17+Q92*Q29*Q18)/Q27 ; dA/dt Q31=(-Q7*Q17-Q8*Q18)/Q27 ; dB/dt P101=Q30*Q93 ; #1 speed in cts/(Isx90 msec) P102=Q31*Q93 ; #2 speed in cts/(Isx90 msec) ELSE ; Near singularity M5182=1 ; Set run-time error bit ENDIF ENDIF CLOSE
-
How can PMAC know that what a speed 1V means?
KiraYamato replied to KiraYamato's topic in Turbo PMAC
Thank you for your explanation. By the way,my Turbo PMAC works in PWM mode, it give the amplifier a analog voltage signal as a velocity command, so PMAC also look at counts only? -
How can PMAC know that what a speed 1V means?
KiraYamato replied to KiraYamato's topic in Turbo PMAC
So, you mean that PMAC never knows how much rpm 1 V means, and how many counts one rev generate? -
How can PMAC know that what a speed 1V means?
KiraYamato replied to KiraYamato's topic in Turbo PMAC
BUT, DO N'T YOU THINK THAT IT WILL RESULT A LONG DYNAMIC PROCESS AND A BAD RESULT FOR A TRAJACTORY FOLLOWING? -
On the page 204 of Turbo SRM, it says that: • I7mn6 = 0: Outputs A and B are PWM; Output C is PWM • I7mn6 = 1: Outputs A and B are DAC; Output C is PWM • I7mn6 = 2: Outputs A and B are PWM; Output C is PFM • I7mn6 = 3: Outputs A and B are DAC; Output C is PFM and according to the page 21 of Turbo PMAC HRM: On Pmac1, there is only one output and one output mode: DAC output. On PMAC2 boards, each channel has 3 outputs, and there are 4 output modes. We know that on the JMACH1,there are DAC1 and DAC1/ pins for channel 1, and there are PUL_1 and DIR_1 on JMACH2 for channel 1. My question is : what do you mean by Outputs A 、B and C? Does A = DAC and B = DAC/ and C=PUL+DIR ? Thank you for your attention
-
Hello, everyone, here I come again~ I am using Turbo Pmac2 Clipper to control Fuji Servo systems, and I set it to work in the analog mode. So the PMAC gives out an analog voltage command which present a rotation velocity but you see that the command in a motion program has the unit of counts/msec, So how can PMAC know that what a speed 1V means? Or How can PMAC know that what a voltage should output when receive a speed command in the unit of cts per second? thank you for your attention~