Jump to content
OMRON Forums

wxswxs1987

Members
  • Posts

    1
  • Joined

  • Last visited

Recent Profile Visitors

The recent visitors block is disabled and is not being shown to other users.

wxswxs1987's Achievements

Newbie

Newbie (1/14)

  • First Post
  • Conversation Starter
  • Week One Done
  • One Month Later
  • One Year In

Recent Badges

0

Reputation

  1. Dear sir, my application-- movement is ball screw feed, driven by AC servo motor, and a linear encoder of 10nm resolution is integrated into the closed-loop feedback. I want to improve the effect of sinusoidal move via adjusting the pid parameters. Step tuning Kp is just 80. Parabolic tuning the entire following error is big, especially on the motor’s directions reversals Sinusodial tuning the following error is so bad on the motor’s directions reversals. can i improve the situation using PMAC,or should i improve the mechanical structure. can any one spare me a help? 3q
×
×
  • Create New...