paison
-
Posts
38 -
Joined
-
Last visited
Content Type
Profiles
Forums
Events
Downloads
Posts posted by paison
-
-
thanks
i set loop for start move Prog1,slove this problem
-
thanks,There is now a problem is in the process of program 1 start setting coordinate system's feedrate is zero,This case is easy to appear can't start,For example:
M5197->X:$002000,24,S
M5197=P1*I10/100 ;
It is easy to appear can't start program 1 when p1 = 0
-
hi,
Present a motion program stopped, I immediately start another Motion Program in the PLC program, find that Motion Program can't start sometimes,For example:
&1
#1->2000X
Open plc1 clear
if(m115=1)
if(Q0=0)
Q0=1
cmd"&1a"
p200 = 1
endif
else
Q0=0
endif
close
Open plc2 clear
if(p200=1)
if(Q1=0)
Q1=1
while(m133=0)
endwhile
cmd"&1B1r"
p200 = 0
endif
else
Q1=0
endif
close
open prog1 clear
inc
linear
Ta(100)
Ts(50)
TM(500)
x(100)
close
-
thanks!!!
-
thanks
-
hi,PMAC how to get Previous move of the command position in real time?
-
I want to realize vector movement, get a sensor signal, immediately with the opposite vector returns specified length, have what good method? Move Until Trigger function can't use here
-
Manual only function parameter function is introduced, I found no range is introduced
-
Thank you, my problem solved
-
Hi,I want to ask DPRSetMem can set how much memory bytes at a time, pcom32 and pcomsever respectively is how much?I found that they are not the same.
-
I would like to know the specific usage of WL, such as:
P1 = 10, p2 = 20, p3 = 30
WL: $6000897093224, 131897093224, 132131413533172
I don't know
10 -- - > 89760930224131
20 -- - > 89760930224132
30 -- - > 131941395335172
Is how convert?
-
I suggest that your project open CLR can work
how ISX13 should be set up?
in Turbo PMAC
Posted
hi,
I urgently want to know how ISX13 should be set up, in my program, there are a lot of very short movement, after opening the Lookahead, feel with & 1 a sometimes can not stop the program