Hello
Ixx66 fonction is not clear for me:
I also have to controle different motors (Brush and brushless motors) with Geo Macro drives. I read the chapter "setting up turbo motor operation"
and as described Ixx66 = 16384 (p. 80, Geo Macro Drive User).
Regarding Sina's answer, I don't really understand the role of Ixx66: For example, my drives input is 230 VAC (then a 325 VDC). Then I should use a transformer for my input voltage in order to controle 110 VDC motors (that was my first idea before I read the spec of Ixx66)?
And I read in Turbo SRM's quote: "If Ixx66 is set to a smaller value than PWM maximum count, it serves as a voltage limit for the motor (Vmax = VDC * PWM_Max_Count / Ixx66)" (source: Software reference manual: Turbo Pmac/Pmac2, p. 106)
I also understand that for Geo Macro, Ixx66 is a constant. So how can I controle the output voltage, if not with Ixx66?
Thank you for your clarification
MH