Jump to content
OMRON Forums

Rendi

Members
  • Posts

    1
  • Joined

  • Last visited

Everything posted by Rendi

  1. Hello guys, I am totally new with PMAC. I have PMAC1 Lite PCI. And, I am just wondering how to generate a sine wave of high frequency (more than 1kHz is good) without a coarseness, and the output voltage is between 0V and 10V. Actually, I already built a code but it is not still satisfied for me. My code is only satisfied for low frequency ranges. Because, I want to drive a piezo actuator in open-loop condition with sine wave of high frequency more than 1kHz using PMAC. Any suggestions are very welcome! Best Regards, Rendi close ;close any buffer opened delete gather ;erase unwanted gathered data undefine all ;erase coordinate definitions in all coordinate systems M102->Y:$C003,8,16,s ;address open plc 1 ;open buffer to be written clear P10=16383 ;define V=5Volt of 16bits P11=1000 ;frequency multiplier P12=360/32767 ;increment, 360 degree is devided by 16bit of 10volt P13=0 ;starting point While (P13 !> 360) M102=cos(P11*P13)*P10+P10 ;output 0V to 10V P13=P13+P12 EndWhile close ;close written buffer, program one
×
×
  • Create New...