Alex
-
Posts
31 -
Joined
-
Last visited
Content Type
Profiles
Forums
Events
Downloads
Posts posted by Alex
-
-
Thanks! Today I'll try it.
Gregs - previous experience I did with the other 60-pin flat cable.
I have two ribbon cable and two terminals ACC-8D.
later I'll write about the results. Regards!
-
Hi!
I did the following:
pulled the computer out of the machine. disconnected the cable from the computer to the PMAС of AСС8D terminal board.
Connect the other does not use the terminal board ACC8D. connect +12 volt to 59-pin. I also joined the "dry contact" switch (http://www.superdroidrobots.com/images/TE-044-000.jpg)
switch is set from 58 pin (AGND) to 52 and 54 pin. switch is normally closed.
Ix225 variable = $C004 and stored in the memory board.
I send a command "Jog" or command "Home".
in the status window, I see the connector pin status change (for motor 2) "motor enable" from red to yellow. when open microswitch status pin "end switches" does not change. :(
I also expect that there should be a red pin "amplifer fault". but it also remains yellow.
-
Hello!
Sina, no :( I do not have a link to the technical documentation of end switches. :(
but they are intact and functioning properly.
I also try to replace one or more limit switches for "dry contact" switch. it just did not have the result: (
Steve.milich - Thanks. I understand correctly, you? - If bit 17 (i25) was set to off, the status of the state of the limit switches is to be displayed. and if bit 17 was ustnovlen to 0 to display the status of the switches must re-activate the motor. otherwise, the status of switches is undefined.
Today I'll be sure to try it. also check the wiring again.
-
HI Sina!
I set the variable ix25 in the correct values. it has no effect. also I change variables i907 and i908 (second channel PMATS). it also has no effect.
if I set the ix25 $C004 the motor does not have any movement. Status window also displays no change in the state limit switches.
http://i42.fastpic.ru/thumb/2012/0906/2f/b732453e3dc2857a3de26125ca46d92f.jpeg http://i42.fastpic.ru/thumb/2012/0906/97/6f04af829a430898800061a03e95ad97.jpeg
Installing variable ix25 is set to $2C004 (do not use limit switches) motor is moving. but also a status window does not display the status change limit switch.
-
Hello DT Support !
if you have a chance, please tell me.
I have PMAC 1.5 + ACC8D. 1.17H
Limit switches are used NC-types:
Switching collected as follows:
http://i40.fastpic.ru/thumb/2012/0905/4f/9d71a38f24f7b575d6059f5a66514f4f.jpeg
I use an external power supply.
I have a problem with the definition of limit switches. system does not have reactions to triggering limit switches. Status window does not display the connector state change switches.
if I'm doing the installation search for "Home" limit switch flag - motor spins endlessly, without response to the state of the switch.
Limit switches are working properly. built-in LED indicates operation of switches. PMAС to change the switch is not responding.
I found a similar topic on the forum. but there PMAC Turbo Clipper card. My board does not have the variable ix24.
What am I doing incorrect?
BEST REGARDS! Alex.
Limit switch problem
in Pre-Turbo PMAC
Posted
Hi!
This attempt was not successful :(
PMAС sees no the state of the limit switches