Jump to content
OMRON Forums

laser3lc

Members
  • Posts

    4
  • Joined

  • Last visited

Everything posted by laser3lc

  1. I get stuck at: Traveled_Distance += sqrt(pow(XAxisPos - PrevXAxisPos,2)+pow(YAxisPos - PrevYAxisPos,2) +pow(ZAxisPos - PrevZAxisPos,2) +pow(BAxisPos - PrevBAxisPos,2) +pow(CAxisPos - PrevCAxisPos,2));
  2. I am looking for some one who had implemented and tested this feature. I try to implement it and get stuck on the page 9 usercode.c
  3. I have the problem or conflict between PowerPmac System Setup and the configuration file. It looks that the save on PowerPMAC does not save the System Setup, and if I open the System Setup and Accept each Motor it will recognize the setup other wise the configuration is not stable some times yes it works and after turn off and On the configuration is not in PPMAc. I am using Absolute Encoders and the plc to read the encoders are working but the Setup and configuration are not. any Idea why? And yes, I update to 1.6 version ,and $$$*** and save and redo a new solution. I need to have very clear why the settings on the System Setup are changing and why the configuration file does not take the system set up file.... The System Setup does not let me Save setup the file.. because is online?
  4. System Set up, helps to define the amplifier, motor, type of encoder... BUT Not the Jog speed, max speed..... that data is done in a Cofiguration file. Now Question how is the interaction between a System set up Motor and the configuration file for that motor?
×
×
  • Create New...