Jump to content
OMRON Forums

Bharat

Members
  • Posts

    1
  • Joined

  • Last visited

Bharat's Achievements

Newbie

Newbie (1/14)

  • First Post
  • Conversation Starter
  • Week One Done
  • One Month Later
  • One Year In

Recent Badges

0

Reputation

  1. Master Motor Reading - Encoder - 10000 cts/rev Max Speed - 300 rpm Slave Motor Reading - Encoder - 10000 cts/rev Ball Screw Pitch - 10 mm/rev of motor I want to run the slave motor, which should starts at 0 degree of master & should stop slave 100 degree of the master. The changing parameter for running the machine are as follows, 1. Slave distance Range - 1 mm to 10 mm 2. Master Speed Range - 1 to 300 rpm Can some body hep me in these to achieve the result to calculate RTIF. I am working Turbo Clipper . Bharat Vinchwekar[/size]
×
×
  • Create New...