I want to run the slave motor, which should starts at 0 degree of master & should stop slave 100 degree of the master. The changing parameter for running the machine are as follows,
1. Slave distance Range - 1 mm to 10 mm
2. Master Speed Range - 1 to 300 rpm
Can some body hep me in these to achieve the result to calculate RTIF. I am working Turbo Clipper .
Time Base - RTIF Calculation
in Turbo PMAC
Posted
Master Motor Reading -
Encoder - 10000 cts/rev
Max Speed - 300 rpm
Slave Motor Reading -
Encoder - 10000 cts/rev
Ball Screw Pitch - 10 mm/rev of motor
I want to run the slave motor, which should starts at 0 degree of master & should stop slave 100 degree of the master. The changing parameter for running the machine are as follows,
1. Slave distance Range - 1 mm to 10 mm
2. Master Speed Range - 1 to 300 rpm
Can some body hep me in these to achieve the result to calculate RTIF. I am working Turbo Clipper .
Bharat Vinchwekar[/size]