pwhiteis
-
Posts
3 -
Joined
-
Last visited
Content Type
Profiles
Forums
Events
Downloads
Posts posted by pwhiteis
-
-
Thanks .. that did the trick. However, the PMAC executive won't talk with the brick any longer. Does it auto-detect the protocol or do I need to tell it which one I'm using?
UDP protocol must be enabled with the “ETHUSBConfigure.EXE” ("Configure USB 2.0" or "Configure Ethernet 100 BaseT" in the common directory) program though a USB connection – there is a radio button to enable this. Note that you must hold in the "BOOT" switch during the enable process untill the application is closed.
-
Hello,
I am writing an application that communicates with the brick using UDP datagrams. The application sends a command and waits for a reply, but always times out. When I setup the socket to use TCP I always get the reply.
Is the UDP protocol always enabled (assuming the IP address is setup correctly), or is this protocol mutually exclusive from TCP?
I have also tried switching between TCP and UDP using the 100 Base T setup utility, but the utility always seems to revert back to TCP. Is the protocol selection stored in EEPROM? I cannot find anything in the Brick Controller Users Manual which speaks to protocol selection.
Thanks,
-Pete-
Setting up Brick Controller for UDP communication
in Turbo PMAC
Posted
Thanks Steve.
Under "General Setup" in PEWin, I do not see a way to communicate USB. It only seems to allow one to insert a device that communicates over Ethernet or standard serial port.
-Pete-