Jump to content
OMRON Forums

johann

Members
  • Posts

    2
  • Joined

  • Last visited

Posts posted by johann

  1. Hi,

     

    Just started using the PPMAC and encountered some errors when running the forward/inverse kinematic subroutines.

     

    The forward routine seems to be working, but when I add the file inverse.kin in the project I encounter buffer related errors (closed, in use, etc). The same error shows up as early as the compiler finds open inverse (1).

     

    I want to know where exactly this error comes from in my project. Is it something I did not define in the forward kinematics routine?

     

    Below is my code for the forward kinematics routine. Am I setting KinAxisUsed correctly? My machine has 5 axes. Thanks!

     

     

    csglobal CtsperMm1;

    csglobal CtsperMm2;

    csglobal CtsperMm3;

    csglobal CtsperDegB;

    csglobal CtsperDegC;

    csglobal Dy; //Y offset//C_B_Dist;

    csglobal Dz; //B_to_Tip_TCP;

    csglobal FwdKinErr;

     

    CtsperMm1 = 1001.16074600000002;

    CtsperMm2 = 1045.03245700000002;

    CtsperMm3 = 1039.48072200000001;

    CtsperDegB = 2912.71111000000019;

    CtsperDegC = 2912.71111000000019;

    Dy = 200; //Y offset//C_B_Dist;

    Dz = 266 ; //B_to_Tip_TCP;

     

    &1 // Address coordinate system 1

    open forward // Open forward kinematics buffer

    if (KinVelEna >0) callsub 100; // Check if double-pass needed, otherwise go to line 100

    KinAxisUsed = $1C6 // Specify X and Y Z B C axes used in inverse kinematics

    n100: // Line label

    if (Coord[1].HomeComplete) // Home complete OK?

    {

    KinPosAxisX = equation;

    KinPosAxisY = equation;

    KinPosAxisZ = equation;

    }

    else // Not valid; halt operation

    {

    if (Ldata.Status & 40) // Called from motion program?

    {

    Coord[1].ErrorStatus = 255; // User-set aborting error

    }

    else // Called from axis query

    {

    KinPosAxisX = sqrt(-1); // Return "not-a-number“ for X axis

    KinPosAxisY = sqrt(-1); // Return "not-a-number“ for Y axis

    KinPosAxisZ = sqrt(-1); // Return "not-a-number“ for Z axis

    }

    }

    return;

    close // Close forward kinematics buffer

  2. I thought that posting the excerpt (attached) from the Power PMAC Training Slides, "Talking to Power PMAC," might be helpful here as a quick reference covering most questions regarding communicating with Power PMAC.

     

    For the rest of the training slides please visit and click Power PMAC-->Training Slides.http://forums.deltatau.com/filedepot/ [FILE REMOVED]

     

    Thanks.

     

    I wonder if it is possible to load programs (and execute them) through telnet or accessing the embedded web server in the Power PMAC...

×
×
  • Create New...