illop
-
Posts
12 -
Joined
-
Last visited
Content Type
Profiles
Forums
Events
Downloads
Posts posted by illop
-
-
This issue is fixed in Power PMAC IDE v4.4.1.7 which is now available on the Omron Website through the "Power PMAC IDE Download" link.
https://automation.omron.com/en/us/products/family/pmac%20ide
Thank you Eric.
-
This problem occurs only in the global include folder.
So now I am working on the PLC PROGRAM folder...
-
Hi Eric
Where can I get some documents or examples related to the logging on USB in C-app?
-
SDO
in Power PMAC
You can access "ecatsdo" function.
ecatsdo
Function: Access an EtherCAT Service Dictionary Object (SDO)
Syntax: ecatsdo ({expression},{expression},{expression},
{expression},{expression},{expression})
The ecatsdo function permits the user to access (write to or read from) the specified EtherCAT Service Dictionary Object (SDO) from within a program.
This function can only be used if Sys.EcatType is set to 0 (Etherlab stack). If Sys.EcatType is 1 (Acontis stack), use the similar ecattypedsdo function.
This function takes 6 arguments.
The first argument is the “direction” of the access. It should be 0 to write to the SDO, or 1 to read from the SDO.
The second argument is the slave index value “j” of the device, corresponding to the structure ECAT.Slave[j] assigned to the device.
The third argument is the index number of the SDO.
The fourth argument is the subindex number of the SDO.
The fifth argument is the data value for the SDO. If the function is used to write to the SDO (first argument = 0), this is the value that will be written, If the function is used to read from the SDO (first argument = 1), this value is not used (but a value must be present here, even if it is unused, in order for the function to execute).
The sixth argument is the master index value “i” (i.e. the EtherCAT network index) of the device, corresponding to the structure ECAT.Slave[j] assigned to the device.
The return value of the function in the case of a valid “read” access is the data value of the specified SDO. The return value in the case of an invalid “read” access is “not-a-number” (nan).
The return value of the function in the case of a valid “write” access is 0. The return value in the case of an invalid “write” access is “not-a number” (nan). Even if the returned value is not really used in the application, it still must be stored somewhere; for example, by assigning it to a “dummy” variable as shown in the example code below.
Example
global sdoresult;
sdoresult = ecatsdo(0,0,$6060,0,10,0); // Write to CAN object
sdoresult = ecatsdo(1,0,$6061,0,0,0); // Read from CAN object
Jaehyuk
-
Hi, All
I want to know status of C-applications(capp1).. in PowerPMAC
(Stop or Running)
How can monitoring in plc program or bgcplc..?
Thanks
-
Hi.
I also experienced the same symptoms in PowerUMAC
In my case,
1)Connect PowerUMAC throught micro-usb
2)delete userflsh folder or rename userflash folder
3) Copying the contents of userflash.1 to userflash
4) clear ^^
-
In my case,
Disconnected PPMAC ISSUE was clear after IP address change.
for example
LAN CARD 1) 192.168.0.2 connected PPMAC
LAN CARD 2) before ->192.168.0.5 after-> 192.168.1.5 connected vision
Thanks
-
Hi~ CharlesP
Look at the image..
derivative gain 1,2 and velocity feed forward 1,2 are different.
That is not problem of no motor enabled.
-
-
Hi CharlesP~
I'm sorry to be late in replying.
There is no problem (I'm just being test- PC to PPMAC direct connect)
About Two month before the issue was not.
But now most PC have same problem.
-
I can't access PPMAC Web
http://192.168.0.200/index.html is same
Connection is no probs.
firmware : 1.5.8.0 and 1.6.0.9
I can see only Title " PPMAC Web - Home"
Other PC result is same..
Comp table bug in the IDE
in Power PMAC
Posted
add
IDE 4.4.1.7
2D- compensation rollover "false"
comptable[m].ctrl = $4 It will be $14.