dcwei
-
Posts
3 -
Joined
-
Last visited
Content Type
Profiles
Forums
Events
Downloads
Posts posted by dcwei
-
-
Hi,
What is the "thread delay period" on the watch window?
(Right-click in watch window, select lowest number)
((You could also prove this by adding Dwells after lines 4,5,6))
Mr P Mac.
Thanks
My watch window thread delay period is 100.
PEWIN32PRO2 said that is the minimum value.
I don't think the problem is the value of thread delay period.
I think the motion program after compiling,the containt has changed.
-
I want to use "PE " command to watch which line of Motion Program is
running.But i have a problem, if the program have "dwell" or at the end of the program ("ret"),the "PE" command will go wrong.
For example
open prog 1 clear Linear ;line 0 ABS ;line 1 TA 500;line 2 TS 250;line 3 x 1000 ;line 4 x -500 ;line 5 x 200 ;line 6 x -1000;line 7 dwell 200 ;line 8 x 1000;line 9 x 0 ;line 10 close
if i run the program,and add "PE" in Watch window,then the line number
will changed from 5 to 8 suddenly.But motion of the moto is normal.
if the Program include P Variable ,“IF……” or “while……” , the line number
will become more strange.
i found that assignment to a P Variable would takes 2 line.
i want to know the reason.
Thanks!
PE problem
in Turbo PMAC
Posted
Thanks
i have got the answer.The PE or List PE command only applies for this application that only contains “X 50 ……Y 30……”