kapadiapj
-
Posts
2 -
Joined
-
Last visited
Content Type
Profiles
Forums
Events
Downloads
Posts posted by kapadiapj
-
-
Does Turbo Clipper support G31 Move Until Trigger function? Is there any sample code I can refer to?
PMAC NC/Turbo Clipper: SKIP position update
in Turbo PMAC
Posted
I have PMAC NC PRO2 and Turbo Clipper Combo (PMAC2). Am trying to install Renishaw probe on the system. I am noticing that I cannot read in commanded work coordinates positions (#5041, #5042, #5043) or current work coordinate skip positions (#5061, #5062, #5063) until we execute M30 or end the program. I need these positions to be updated in real time as soon as the SKIP is triggered for the probe to work. The SKIP signals for X, Y and Z axes are hard-wired to USER Input on JMACH2 Port. G31 seems to be working - it is just the update part I am struggling with.
Below is the code I am using to test and monitoring values on Data Pages for Common Variable on PMAC NC PRO2 HMI.
(Probe face 10" pipe
G103P1
G20
G90G00G54X0Y0Z0
M51
G4P2.0
#500=#5041
#501=#5042
#502=#5043
G90G31X1.0Y1.0Z1.0F10.0
G4P2.0
#504=#5041
#505=#5042
#506=#5043
#507=#5061
#508=#5062
#509=#5063
M30
...... any ideas?