Kit Richrds
-
Posts
4 -
Joined
-
Last visited
Content Type
Profiles
Forums
Events
Downloads
Posts posted by Kit Richrds
-
-
I'm trying to use the plot feature of the PPMAC IDE. The gather button seems to work but the upload button never finishes. I have a very simple setup sampling motor 8 actpos, despos, iqcmd, processing motor 8 cmd position, following error. Plotting following error on left axis, cmd position on right axis. Max gather samples 10, sample period 10. The window says Legacy Mode in the lower left corner.
Any ideas why it is unable to upload the sampled data?
Thanks!
-
I would like to be able, via the IDE, to set a motor so the homecomplete indication is false. Is there way to do that? PPMAC, ACC-24E3. Thanks!
-
I need to make schematics and drawings of a system with 26 small motors. I have been given a quote for DeltaTau and Copley equipment to accomplish this but am not finding documentation for some of the Delta Tau equipment. Can someone point me to manuals/drawings for the following?
300-603490-10x
Delta Tau
AMP-4-1-BP, Analog Amplifier Single Backplane Board.
3-2932A-01-2100-B000
Delta Tau
ACC-D3, 21-slot 3U rack. 17.00"Wide x 8.75" Deep X
5.20"High (BLACK plates)
5-4269-00-1821-B0100
Delta Tau
Integrated UMAC Rack w/18-Slot Backplane, 21 slot
rack & power supply, Black Plates
Thanks!
plot upload fail
in Power PMAC
Posted