Hi,
I am studying the Power PMAC Etherlite and Power Brick AC. I would like to link them together using MACRO, is the fiber inside the package ? If not I can't find the information about where one can find it.
I have also some (maybe really debutant) questions:
- We need a 24 VDC supply quite often, if we use only one for all the requirements (Brake Power, STO and for the Etherlite), do you have some advice on one specific generator supply to do so?
- What is the +24 VDC RET?
- Do one need to order all the connectors from Phoenix?
- Is there any website on which we can order all the D-sub needed?
I would like to use an encoder and the output signal is square signals but this is not digital. Should I use a ADC and then the Encoder X1 or can I use the analog input ?
Thank you in advance,
Matthieu