thamwaifoong
-
Posts
2 -
Joined
-
Last visited
Content Type
Profiles
Forums
Events
Downloads
Posts posted by thamwaifoong
-
-
Hello guys,
i have directly connected a maxon flat motor come with a MILE (inductive incremental encoder) to J3 terminal from turbo pmac clipper board, but there's no position ready. When i changed back to HEDS 5540 avago optical encoder, everything works fine. The conversion type is 1/T extension of incremental encoder. May i know where i did wrong?
attached the motor and encoder datasheet.
Thanks.
Ethernet connection with Arduino
in Turbo PMAC
Posted
Hello,
I have a setup of Turbo PMAC with Arduino.
With the arduino mega board, i have stacked with ethernet shield with it.
I've setup the PMAC ip address (169.254.16.195) and a default port no (1025).
Mode: TCP, board: PC104.
And the arduino ip address is 169.254.16.194, as client.
i don't see the ethernet port LED lighting up on both devices (PMAC or Arduino).
if i plug PMAC to computer, i can see the ethernet port lighting up. Same as arduino board, when i plug the ethernet from arduino to computer, it lights up too. but when i connect from pmac to arduino, no sign of any indication.
Is there anything i've missed?
i would like to use the arduino board to send simple commands like p23=100.