Running Turbo PMAC on GEO Brick controlling a Dover stage. One of the 5 stages we have is having problems. All stages are running the same code.
An error happens approximately once every 10 minutes of continuous motion.
The error is Amplifier Fault Error (Bit 3), Open Loop Mode, Also the Abort Deceleration in progress bit comes on.
There seems to be no resistance when moving the stage by hand.
Is there any diagnostics we can run, other error bits or anything else to narrow down what the problem source is?
Motors, Scales, Wiring, Physical Obstruction, Bad Tuning???