Jump to content
OMRON Forums

killerisation

Members
  • Posts

    2
  • Joined

  • Last visited

killerisation's Achievements

Newbie

Newbie (1/14)

  • First Post
  • Week One Done
  • One Month Later
  • One Year In
  • Conversation Starter

Recent Badges

0

Reputation

  1. I assumed that I could copy the .cfg file from my 4-axis pmac to my 8 axis one and my channels 1-4 would work the same. This post suggests it should: http://forums.deltatau.com/showthread.php?tid=261&pid=645#pid645 Unfortunately it doesn't. As I move the motors by hand I see a correct change in position but when using the jog ribbon I can just feel an occasional small pulse, esp when I hit the Kill All button. Programs don't run at all. What parameters do you think need changing?
  2. Hi, I have a XYZ table that uses brushed motors that is working nicely, but I want to add another (rotary, stepper motor) axis and I need help setting it up. I believe I have all the right hardware, which consists of: - NEMA 23HD450Y-31A6 stepper motor - Single Axis 4A TB6600 Hybrid Stepper Motor Driver - Meanwell S-50-12 12v power supply - Accessory 8D breakout board with Option 2A V-F converter - 8-axis PMAC-PCI v105B - PEWin32Pro2 v4.4.0.0 running on Windows XP At present the terminal says "Communication Established to PMAC-0" but I am unsure what parameters to set and the 500+pg manual looks pretty daunting. Thanks in advance.
×
×
  • Create New...