londors
-
Posts
8 -
Joined
-
Last visited
Content Type
Profiles
Forums
Events
Downloads
Posts posted by londors
-
-
I am unable to connect to the Power Clipper.
I can ping it fine but every time I try to connect with the IDE i get an error message saying one of the following:
Power PMAC connection faild for the device . Please check login parameters and try again.
or
Gpascii connect failed for the device . Please Cycle power device and then reconnect. If the problem persists then please contact Delta Tau Support.
So I have tried power cycling it many times and get the same problem every time. I tried a different Ethernet cable but I can still ping the device fine so it must be a hardware/software issue with the Power Clipper.
I looked on the forum but was unable to find information on how to flash the Power Clipper via a USB pen. I also saw something that mentions resetting back to factory settings if the E3 jumper is used but there does not seem to be an E3 jumper on my Power Clipper.
So for now it is an expensive paperweight as it refuses to connect to the IDE.
-
As no one could resolve this I had to get a new laptop
-
Reply to AAnikstein:
When opening a new terminal i just get another grey box that has a title of "Power Pmac". (So yes to your question, I do get another grey box)
I have performed many fresh installs. I have tried selecting "No Device" and still I get a grey box instead of a terminal.
-
Reply to steve.milici:
I tried this but still have the same issues
-
I see you did not understand my previous message. I have already tried with "No Device" and still Power PMAC does not work correctly.
The Terminal window is always incorrect as can be seen in the screenshot in the first post. (I am unable to add another as there is no option for this in the comment section)
-
Even without connecting to a device Power PMAC is not running correctly. The Terminal window never works. I am using the latest version of Power PMAC i.e. 2.1.0.107
-
I have installed Power PMAC as administrator, I have entered an IP on startup so it will link to a VM. This is all ok but when the Power PMAC Suite opens the Terminal window is not working and the Watch window causes a crash if you try to remove the Sys.ServoCount command. Also the watch window seems to always have a windows loading mouse cursor.
I have reinstalled many times but I still get the same issues every time I start Power PMAC up and connect it to a VM.
PC Specs:
OS: Win 7 Pro 64-bit
CPU: Intel Core i-7-3840QM 2.8GHz
RAM: 8GB
SSD drive with ample space
Power Clipper
in Power PMAC
Posted
Great. The "PowerPmacFactoryReset" option worked. Now I can reconnect to the Power Clipper.
Thanks for the help.