Hi,
I am trying to build and download a project that I have had working (building and downloading fine) previously from a different computer.
I have copied the project files over to a new computer, and when I try to build and download from this computer, I get a build failure with the following output:
'Please wait while Executing Project Script.
Please wait while mapping Power PMAC variables.
End of syncing the database.
PMAC variables are mapped successfully.
Build Process For usralgo.ko has started.
C:\PPMAC MiniGST\PowerPmac1\PowerPmac1\PowerPmac1.ppproj(176,5): Error : make: /bin/sh: Command not found
C:\PPMAC MiniGST\PowerPmac1\PowerPmac1\PowerPmac1.ppproj(176,5): Error : make: /bin/sh: Command not found
C:\PPMAC MiniGST\PowerPmac1\PowerPmac1\PowerPmac1.ppproj(176,5): Error : make: /bin/sh: Command not found
Build Process For usralgo.ko has ended.
Build Process For usralgo.so has started.
Build Process For usralgo.so has ended.
Done building project "PowerPmac1.ppproj" -- FAILED.'
the errlog for the realtime routines - which i think this is linked to since it fails during the usralgo.ko build is as follows:
'make: /bin/sh: Command not found
cp: missing destination file operand after '/usr/local/usralgo/usralgomain.c'
Try 'cp --help' for more information.
make: *** [all] Error 1'
as far as I am aware this usralgomain.c is a default file that has not changed between the two computers,
if anyone has seen this error before, and can point me in the right direction as to what I am doing wrong, it would be appreciated,
Colin