Jump to content
OMRON Forums

rhenning

Members
  • Posts

    2
  • Joined

  • Last visited

rhenning's Achievements

Newbie

Newbie (1/14)

  • First Post
  • Week One Done
  • One Month Later
  • One Year In
  • Conversation Starter

Recent Badges

0

Reputation

  1. Hi, I would like to setup an electronic cam and I'm not sure if it is possible to do with my current setup. I have a Turbo PMAC2 Clipper with two stackable boards (ACC51S and ACC-8ES) with 4 servo motors connected. From what I've read it sounds like I need to connect my external frequency to an incremental encoder input. Since I'm using the 4 original channels for my motors I was wondering if the handwheel inputs could be used. If so then is there any more information available than what's in the manual. Thanks!
  2. Hello! First time poster here. I have a situation where I need to synchronize a series of motor positions with an external timing event but I can not precisely control when the external event will happen. I can send a series of pulses to the PMAC for synchronization but I'm not sure how to make sure everything is in sync. I have already written code to do this asynchronously but I didn't have to worry about the timing in the initial setup. More details! I have a series of X-ray pulses (~100 but it varies) that need to hit my sample at specific positions (~0.2 mm apart but that can vary as well). Each X-ray pulse has to hit a different spot on my sample. The pulses come at a rate of about 10 Hz. The motor motion is usually just linear and I want it to be a continuos motion through all of the motor positions. I know that a stepped motion would be easier to implement but I have problems with sample vibrations that limit my speed to 2 or 3 Hz. I'm thinking about sending a separate pulse train to the PMAC that will provide the timing of the pulses and then send a different pulse to actually trigger the motion. I'm just not sure how to do the synchronization. I have Turbo PMAC2 if that matters. Thanks for the help!
×
×
  • Create New...