rhenning
-
Posts
2 -
Joined
-
Last visited
Content Type
Profiles
Forums
Events
Downloads
Posts posted by rhenning
-
-
Hello! First time poster here.
I have a situation where I need to synchronize a series of motor positions with an external timing event but I can not precisely control when the external event will happen. I can send a series of pulses to the PMAC for synchronization but I'm not sure how to make sure everything is in sync. I have already written code to do this asynchronously but I didn't have to worry about the timing in the initial setup.
More details! I have a series of X-ray pulses (~100 but it varies) that need to hit my sample at specific positions (~0.2 mm apart but that can vary as well). Each X-ray pulse has to hit a different spot on my sample. The pulses come at a rate of about 10 Hz. The motor motion is usually just linear and I want it to be a continuos motion through all of the motor positions. I know that a stepped motion would be easier to implement but I have problems with sample vibrations that limit my speed to 2 or 3 Hz.
I'm thinking about sending a separate pulse train to the PMAC that will provide the timing of the pulses and then send a different pulse to actually trigger the motion. I'm just not sure how to do the synchronization.
I have Turbo PMAC2 if that matters.
Thanks for the help!
Electronic cam
in Turbo PMAC
Posted
Hi,
I would like to setup an electronic cam and I'm not sure if it is possible to do with my current setup. I have a Turbo PMAC2 Clipper with two stackable boards (ACC51S and ACC-8ES) with 4 servo motors connected.
From what I've read it sounds like I need to connect my external frequency to an incremental encoder input. Since I'm using the 4 original channels for my motors I was wondering if the handwheel inputs could be used. If so then is there any more information available than what's in the manual.
Thanks!