seanxyuan
-
Posts
4 -
Joined
-
Last visited
Content Type
Profiles
Forums
Events
Downloads
Posts posted by seanxyuan
-
-
Have you set Coord[x].SegMoveTime to a value greater then zero?
Thanks for your response. I set Coord[1].SegMoveTime=10 and still it moves linear not circular. Is there any other parameter that I should change to have a circular move for X and Y?
-
I am trying to create a circle move (1 quarter - 90 degrees) using the prog1.pmc code as below:
undefine all
&1
#1->1711025 X
#8->1365276 Y
#2->2105867 Z
#7->393216 a
open prog 1
ta 125
ts 35
tm 1000
dwell 2000
G17
G91
G02 X0.25 Y0.25 I0.25 J0.25
close
For G-Code commands, I have also created subprog1.pmc as follow:
open subprog 1000
N0: rapid return;
N1000: linear return;
N2000: circle1;return;
N3000: circle2 return;
N9000: dwell 10 return;
N17000: normal K-1 return;
N18000: normal J-1 return;
N19000: normal I-1 return;
N90000: abs return;
N91000: inc return;
close
However, the output is just a LINEAR movement from current position to point (0.25,0.25). I tried several other ways, such as using circle1 directly in my prog1.pmc but none of them worked.
Can anyone help what might be the issue here?
Thanks,
-
Were you able to solve this issue using Paramiko and Python3?I am also able to run commands like "ls" but when I send the ''gpascii' command it hangs there. Any suggestions?
Connection Issue to Controller for Power PMAC
in Power PMAC
Posted
Our system was working properly but we cannot connect to Power PMAC controller any more. We get the following message:
"Can not add the device 192.168.0.200 to network route".
One of our PCs is still able to connect but the other one cannot. Is it related to windows automatic update maybe? Has anyone faced the same issue before?
This is urgent. I appreciate your help.