glennstanley
-
Posts
5 -
Joined
-
Last visited
Content Type
Profiles
Forums
Events
Downloads
Posts posted by glennstanley
-
-
My problem continues. RY gets me 0. No change.
I see PEWin32Pro2 reports in the terminal header
Terminal: Device #0 [QMAC TURBO]V.1947
I think it be "GEO Brick Drive" instead of QMAC.
What do I do now?
How do I confirm it might REALLY be a QMAC?
-
M var assignment should work. You can look at the coordinate system status in the Pewin. You can issue RY:$2014 in the terminal window.
Can you enable with #nO0?
Do you have feedback?
How are you phasing?
What hardware do you have?
$$$*** deletes commutation parameters!
What is RESET?
What LED and +5 are you referring to?
New or existing installation?
I attempted to phase using #1$
RY gets me 0
I tried #1o0 and get
"attempt to perform phase reference during move, move during phase reference, or enabling with phase clock error"
This is a GBL4-CO-505-??D
We attempted hardware RESET on outside of GEO Brick chassis
These LEDS are under the (D10) 7-segment display
There are 4 LEDS. I don't have a WD (Watch Dog) glowing LED
This config file was running for some time until now.
It is in the field.
I don't have any LIMITS set for any axis.
-
...Can’t phase a thing
Yet there are no limits on any of axes 1-4.
I can't remember how to poke register Y:$002014.
tried with MVar M1000->Y:$002014 but that does not work
I also tried RESET
LED INACTIVE and +5 are glowing
My customer reports that he does not see anything on 7-segment (D10) display
Also did $$$***
I also cycled power.
-
Brick responds with E0000000 error after attempt to phase any axis. However, no axis has limits violation. Could this be a runt-time error of sorts?
Axis Phase error E000000
in Turbo PMAC
Posted
With the assistance of your support staff via telephone, we have concluded that the Geo Brick AC internal amplifier has failed. Unit does not replay to
ampver
ampmod
only produces and error message.
The unit is being prepped for rma
Thanks.