Jump to content
OMRON Forums

awhitebwcutters.com

Members
  • Posts

    2
  • Joined

  • Last visited

  • Days Won

    1

awhitebwcutters.com last won the day on February 15

awhitebwcutters.com had the most liked content!

Recent Profile Visitors

The recent visitors block is disabled and is not being shown to other users.

awhitebwcutters.com's Achievements

Newbie

Newbie (1/14)

  • First Post
  • Week One Done
  • One Month Later
  • One Year In
  • Conversation Starter

Recent Badges

1

Reputation

  1. I am setting up 6 Sanyo Denki Series 3 drives to CK3E controller. The XML files have been loaded to the IDE. As I add the drives to the project and scan ethercat network I get the above error. I tried changing firmware on drives but the error remains. The project is correct as works fine on another system. Trying to create an identical system this error message persists. Can anyone advise please?
  2. I'm surprised by this, supporting DotNetCore would be a big win as it enables cross platform support. Running the Portability Analyzer on this (see attached output) it doesn't look like too big a job - 9/13 dll's are 100% compatible. The worst of the rest is 89% compatible. for the remainder: Prism - new versions support .net standard Microsoft.Build.Utilities - a .net core version now exists https://www.nuget.org/packages/Microsoft.Build.Tasks.Core/ Renci.ssh - you may need to switch ssh libraries but since ssh is a standard protocol it should be fine Hope you decide to undertake it in the near future and good luck if you do
×
×
  • Create New...