Hi, I want to share the problems and solutions I had for other people to benefit from it. So the problem is solved.
Problem: When building and downloading an empty
Powerbrick Solution Template I get the Message:
error : The compiler was not able to generate an executable file. Please open the following error log file for more information
Output:
********************************************************
********************************************************
Please wait while uploading Libraries from PowerPMAC.
Libraries upload successful.
Please wait while Executing Project Script.
Please wait while mapping PowerPMAC variables.
End of synchronizing the Database.
PowerPMAC variables mapped successfully.
Build process for capp1.out has started.
\\win.desy.de\home\guickinf\My Documents\PowerPMAC IDE\PowerBrick_LV1\PowerBrick_LV1\PowerBrick_LV1.ppproj(94,5): error : The compiler was not able to generate an executable file. Please open the following error log file for more information
\\win.desy.de\home\guickinf\My Documents\PowerPMAC IDE\PowerBrick_LV1\PowerBrick_LV1\C Language\Background Programs\capp1\err.log
\\win.desy.de\home\guickinf\My Documents\PowerPMAC IDE\PowerBrick_LV1\PowerBrick_LV1\C Language\Background Programs\capp1\msg.log
Build process for capp1.out has ended.
Done building project "PowerBrick_LV1.ppproj" -- FAILED.
Project Building and Mapping total time = 4.132 sec
========== Build: 0 succeeded or up-to-date, 1 failed, 0 skipped ==========
********************************************************
********************************************************
However when I used an sftp-file transfer software to manually copy the files onto the PowerBrickLV
it works and I can run the Motion Program. As soon as I do a Factory Reset it is of course gone.
When I try to upload motion programs it gives me the information:
Error message: Project Load Error
Output:
********************************************************
********************************************************
Total Project download time = 3.572 seconds.
Total Project build and download time = 4.777 seconds.
There were errors during the download process and the download process has stopped.
The following errors were found:
Error: Opening PMAC File: /var/ftp/usrflash/Project/PMAC Script Language/Global Includes/global definitions.pmh
Error: Opening PMAC File: /var/ftp/usrflash/Project/PMAC Script Language/Libraries/poweronresetsub.pmc
Error: Opening PMAC File: /var/ftp/usrflash/Project/PMAC Script Language/Libraries/timersub.pmc
Error: Opening PMAC File: /var/ftp/usrflash/Project/PMAC Script Language/Motion Programs/prog1.pmc
Error: Opening PMAC File: /var/ftp/usrflash/Project/PMAC Script Language/PLC Programs/plc1.plc
Build Succeeded.
********************************************************
********************************************************
Solution: My Project-Folder was automatically created on a network drive.
On other systems this may not be a problem, but in my case it was.
The support found out that it was caused by my pc, not allowing for the long path names
arising from the location of the project on the network drive.
Many thanks to the Support for helping me out!
Easy workaround: Save your Project on your local disk.
Fixing it: This are the Instructions given by the support. I wasn't able to specify
a certain drive, so I had to set the value to "0" for all drives.
********************************************************
********************************************************
1) As Administrator (right click on CMD icon, “ Run as Administrator” ), you have to query the short name path status for that drive
C:\WINDOWS\system32>fsutil 8dot3name query d:
You will probably see the following:
The volume state is: 1 (8dot3 name creation is disabled).
The registry state is: 2 (Per volume setting - the default).
Based on the above two settings, 8dot3 name creation is disabled on d:
2) In this case you have to enable the short path with the following command:
C:\WINDOWS\system32>fsutil 8dot3name set d: 0
Successfully enabled 8dot3name generation on d:
C:\WINDOWS\system32>fsutil 8dot3name query d:
The volume state is: 0 (8dot3 name creation is enabled).
The registry state is: 2 (Per volume setting - the default).
Based on the above two settings, 8dot3 name creation is enabled on d:
Nota bene: Maybe you have to zip all the projects files, remove or move the original files and unzip the files to let windows to regenerate the short name path, but first see if everything works without this additional step.
Important: remember to map the folder with the projects and do not browse the network server from the file selector. For certain reasons, if you load the solution from the network servers instead from a mapped share drive, you will get a garbled solution explorer, with several folder entry repeated x times.
********************************************************
********************************************************
That both worked fine and the empty Template, as well as the Motion Program gave me the output I wished for:
********************************************************
********************************************************
Please wait while uploading Libraries from PowerPMAC.
Libraries upload successful.
Please wait while Executing Project Script.
Please wait while mapping PowerPMAC variables.
End of synchronizing the Database.
PowerPMAC variables mapped successfully.
Build process for capp1.out has started.
Build process for capp1.out has ended.
Project Building and Mapping total time = 5.409 sec
========== Build: 1 succeeded or up-to-date, 0 failed, 0 skipped ==========
********************************************************
********************************************************
Please wait while uploading Libraries from PowerPMAC.
Libraries upload successful.
Please wait while Executing Project Script.
Please wait while mapping PowerPMAC variables.
End of synchronizing the Database.
PowerPMAC variables mapped successfully.
Project Building and Mapping total time = 3.826 sec
Please wait while downloading to PowerPMAC.
sending incremental file list
./
deleting Temp/pp_debug.txt
deleting Temp/
deleting Database/pp_subprog.sym
deleting Database/pp_prog.sym
deleting Database/pp_local.sym
deleting Database/pp_global.sym
deleting Database/
PowerBrick_LV_Filip_6.ppproj
5,554 100% 0.00kB/s 0:00:00
5,554 100% 0.00kB/s 0:00:00 (xfr#1, to-chk=34/36)
Bin/
deleting Bin/Release/
Bin/Debug/
deleting Bin/Debug/usralgo.so
deleting Bin/Debug/usralgo.ko
C Language/
deleting C Language/Libraries/
C Language/Background Programs/
C Language/Background Programs/capp1/
C Language/CPLCs/
deleting C Language/CPLCs/user/
deleting C Language/CPLCs/rti/
C Language/CPLCs/bgcplc00/
C Language/CPLCs/rticplc/
C Language/Include/
deleting C Language/Include/pp_proj.h
C Language/Realtime Routines/
deleting C Language/Realtime Routines/.tmp_versions/
Configuration/
Configuration/pp_custom_save.cfg
235 100% 11.47kB/s 0:00:00
235 100% 11.47kB/s 0:00:00 (xfr#2, to-chk=19/36)
Configuration/pp_custom_save.tpl
0 100% 0.00kB/s 0:00:00 (xfr#3, to-chk=18/36)
Configuration/pp_disable.txt
248 100% 12.11kB/s 0:00:00
248 100% 12.11kB/s 0:00:00 (xfr#4, to-chk=17/36)
Configuration/pp_inc_disable.txt
0 100% 0.00kB/s 0:00:00 (xfr#5, to-chk=16/36)
Configuration/pp_inc_startup.txt
0 100% 0.00kB/s 0:00:00 (xfr#6, to-chk=15/36)
Configuration/pp_proj.ini
700 87% 34.18kB/s 0:00:00
796 100% 38.87kB/s 0:00:00 (xfr#7, to-chk=14/36)
Configuration/pp_save.cfg
32,768 27% 1.56MB/s 0:00:00
119,934 100% 5.72MB/s 0:00:00 (xfr#8, to-chk=13/36)
Configuration/pp_startup.txt
0 100% 0.00kB/s 0:00:00 (xfr#9, to-chk=12/36)
Documentation/
Documentation/note.txt
0 100% 0.00kB/s 0:00:00 (xfr#10, to-chk=11/36)
Log/
Log/pp_error.log
15 100% 0.73kB/s 0:00:00
15 100% 0.73kB/s 0:00:00 (xfr#11, to-chk=10/36)
Log/pp_proj.log
3,270 100% 159.67kB/s 0:00:00
3,270 100% 159.67kB/s 0:00:00 (xfr#12, to-chk=9/36)
PMAC Script Language/
deleting PMAC Script Language/Kinematic Routines/
PMAC Script Language/Global Includes/
PMAC Script Language/Global Includes/global definitions.pmh
0 100% 0.00kB/s 0:00:00 (xfr#13, to-chk=4/36)
PMAC Script Language/Libraries/
PMAC Script Language/Libraries/poweronresetsub.pmc
1,954 100% 95.41kB/s 0:00:00
1,954 100% 95.41kB/s 0:00:00 (xfr#14, to-chk=3/36)
PMAC Script Language/Libraries/timersub.pmc
685 100% 33.45kB/s 0:00:00
685 100% 33.45kB/s 0:00:00 (xfr#15, to-chk=2/36)
PMAC Script Language/Motion Programs/
PMAC Script Language/Motion Programs/prog1.pmc
773 100% 37.74kB/s 0:00:00
773 100% 37.74kB/s 0:00:00 (xfr#16, to-chk=1/36)
PMAC Script Language/PLC Programs/
PMAC Script Language/PLC Programs/plc1.plc
341 100% 16.65kB/s 0:00:00
341 100% 16.65kB/s 0:00:00 (xfr#17, to-chk=0/36)
sent 20,299 bytes received 1,001 bytes 14,200.00 bytes/sec
total size is 133,805 speedup is 6.28
Downloading pp_startup.txt to PowerPMAC.
Downloading pp_disable.txt to PowerPMAC.
Downloading pp_custom_save.tpl to PowerPMAC.
Downloading pp_proj.ini to PowerPMAC.
Please wait while loading the project.
LoadRTUserCode() Delta Time (sec) = 0.052814Start of Project Loading using INI File: "/var/ftp/usrflash/Project/Configuration/pp_proj.ini"Status: Starting Pass #1, getting Script properties & file names
Status: Pass #1, Pre-processing file: /var/ftp/usrflash/Project/PMAC Script Language/Global Includes/global definitions.pmh
Status: Pass #1, Pre-processing file: /var/ftp/usrflash/Project/PMAC Script Language/Libraries/poweronresetsub.pmc
Status: Pass #1, Pre-processing file: /var/ftp/usrflash/Project/PMAC Script Language/Libraries/timersub.pmc
Status: Pass #1, Pre-processing file: /var/ftp/usrflash/Project/PMAC Script Language/Motion Programs/prog1.pmc
Status: Pass #1, Pre-processing file: /var/ftp/usrflash/Project/PMAC Script Language/PLC Programs/plc1.plc
Status: Pass 1 Create debug file, #defines, *.h & .sym files, Time (sec) = 0.026702
Status: Pass 2 Verify prog calls, local stack & labels, Time (sec) = 0.001391
Status: Create PPMAC Symbol Table & Run CPP Time (sec) = 0.194447Status: Downloading to Power Pmac file = /var/ftp/usrflash/Temp/pp_proj.pmaStatus: Download to PPMAC Command Processor, Time (sec) = 0.002097
Status: Final pp_proj.h & Run Background C Apps, Time (sec) = 0.056196Project Preprocessing & Load Total Time (sec) = 0.333942
Success: projpp
projpp-completed
Uploading pp_error.log file from the PowerPMAC.
Uploading pp_proj.log file from the PowerPMAC.
Uploading pp_error_hist.log file from the PowerPMAC.
Uploading pp_debug.txt file from the PowerPMAC.
Uploading pp_proj.h file from the PowerPMAC.
Uploading and synchronizing PowerPMAC variables
Download successful.
Total Project download time = 3.838 seconds.
Total Project build and download time = 7.664 seconds.
Build Succeeded.
********************************************************
********************************************************