sushant.dighe
-
Posts
4 -
Joined
-
Last visited
Content Type
Profiles
Forums
Events
Downloads
Posts posted by sushant.dighe
-
-
I have fresh power PMAC controller
1.when i'm start first time motor(#1j+/#1j-) is working fine.
2.when i use some unwanted command on motor that time PWR LED is off and motor not working . And error showing Motor not active ( then i check in troubleshooting why motor is not running there shows motor[x].ServoCtrl is wrong value set but these value set automatically then i correct this error and once again write the command #1j+/#1j- that time i get the motor[x].FeFatal error how to resolve this issue ?
3.now i need to how to run motor continues ?
4.see below program
// &1 // Address C.S. 1
// #1->1000X // Motor 1 assigned to X-axis, 1000 counts/unit
// Motion program code
open prog 1 // Open buffer for entry
linear; // Linear interpolation move mode
abs; // Absolute move mode
ta500; // 1/2-second accel/decel time
ts0; // No S-curve accel/decel time
f5; // Speed of 5 axis units per time unit
X10; // Move X-axis to position of 10 units
dwell500; // Sit here for 1/2-second
X0; // Move X-axis to position of 0 units
dwell500; // Sit here for 1/2-second
close // Close buffer, end program entry
how to run above motion program code
Motor not working properly
in Power PMAC
Posted