Jmurphy Posted June 15 Share Posted June 15 I have the Ethernet/IP Activated on the Brick but and getting an IOI Syntax Error when trying to read the output array. Data type: DINT 4byte Output[25] Data type: DINT 4byte Input[25] I have and Explicit UDP CIP Data Table Read Connection Path: 2,IP Address Source Element: Eip.Connection[0].Output.Idata[0] Number of Elements: 25 Destination Element: EIP_Output DINT[25] I also tried with a Generic Ethernet Module Input and Output Instances as Listed on the EIP Tab Output 25x32 bit Input 25x32 bit Configuration 1 0x8bit Is there and AOP or an EDS for this hardware to directly connect to a Rockwell Automation PLC or will this have to be handled in a standalone application or would it be better to create a Logix Socket for communication? Thank you Quote Link to comment Share on other sites More sharing options...
Recommended Posts
Join the conversation
You can post now and register later. If you have an account, sign in now to post with your account.