wbzhong Posted November 17 Share Posted November 17 Hi, when we run "ecat reset" in the terminal, it reports an error: error#20: illegal cmd: ecat 3 Could you give us some insights in the error? Quote Link to comment Share on other sites More sharing options...
Gregs Posted November 17 Share Posted November 17 That error is reporting that you typed ecat "3", not ecat reset. It would seem that somewhere in the project there is a #define statement defining reset as "3", i.e. #define reset 3. I would look in Global Includes first. Or, ctrl-F to search in the project. Quote Link to comment Share on other sites More sharing options...
Alex Anikstein Posted November 20 Share Posted November 20 To add on a tiny bit-- While it is allowed, it is generally considered bad practice to have short words like that (reset, status, etc.) as #defines or variable names. Any string which is either a command or part of a command (for instance, a variable named "AbsPos" would be considered part of Motor[x].AbsPosSf) should be avoided. A better option would be to name your parameter "ResetVar" if it is a variable or "_reset" if it is not. This way it is similar, but unique. Quote Link to comment Share on other sites More sharing options...
wbzhong Posted November 24 Author Share Posted November 24 On 11/20/2023 at 6:25 PM, Alex Anikstein said: To add on a tiny bit-- While it is allowed, it is generally considered bad practice to have short words like that (reset, status, etc.) as #defines or variable names. Any string which is either a command or part of a command (for instance, a variable named "AbsPos" would be considered part of Motor[x].AbsPosSf) should be avoided. A better option would be to name your parameter "ResetVar" if it is a variable or "_reset" if it is not. This way it is similar, but unique. Thanks for the comments. It turned out that I named a PLC "reset", and this PLC was assigned an ID of 3 by the IDE. Quote Link to comment Share on other sites More sharing options...
Eric Hotchkiss Posted Tuesday at 09:02 PM Share Posted Tuesday at 09:02 PM You can name the PLC something like "ResetPLC" to keep the descriptive name and avoid the short word issues. Quote Link to comment Share on other sites More sharing options...
Recommended Posts
Join the conversation
You can post now and register later. If you have an account, sign in now to post with your account.