Shreyas D Posted December 8, 2023 Share Posted December 8, 2023 Hello All, I am very much new to PMAC & Delta-Tau Products Right now, I am using Omron 1S Drive (Absolute Multiturn Encoder) along with CK3E Controller firmware version 2.7. 0.0 I need to understand how to do Absolute homing. Can you please help me with some project examples? This would be great support. I will wait for reply. Quote Link to comment Share on other sites More sharing options...
Gregs Posted December 8, 2023 Share Posted December 8, 2023 See the attached document. Note that I did some testing with that procedure, and I had some trouble when I ran the PLC again with the axis in different positions. There was a problem with the stored home position. I remedied that with some code that used the HomeOffset to compensate for the last stored home position. The code I added is in the two commented out sections here: open plc Mot5AbsPos LOCAL Direction //Is the drive set as CW+ or CCW+ /* local OldHomePos, HomePosDiff, HomeOffsetSetting HomeOffsetSetting=Motor[5].HomeOffset // Store HomeOffset Motor[5].HomeOffset=0 OldHomePos=Motor[5].HomePos */ Sys.Udata[13] = ecattypedsdo(0,0,1,$4510,$84,0,$4) sys.Idata[14] = ecattypedsdo(0,0,1,$4510,$85,0,$4) Direction = ecattypedsdo(0,0,1,$3000,1,0,4) CALL Timer(0.050) Motor[5].AbsPosSf = ((2 * Direction) - 1) * Motor[5].PosSf CALL Timer(0.050) HOMEZ 5 /* CALL Timer(0.050) Motor[5].HomeOffset = HomeOffsetSetting + OldHomePos - Motor[5].HomePos // Restore HomeOffset and add in the change in HomePos HOMEZ 5 CALL Timer(0.050) Motor[5].HomeOffset = HomeOffsetSetting // Restore proper setting */ DISABLE PLC Mot5AbsPos CLOSE Absolute Homing a 1S Drive over EtherCAT.pdf Quote Link to comment Share on other sites More sharing options...
Recommended Posts
Join the conversation
You can post now and register later. If you have an account, sign in now to post with your account.