lithish Posted January 20 Share Posted January 20 need help in setting up servo motor in omron ck3m with closed loop servo control using sd700 veichi servo driver and motor. setup available omron ck3m with 4 channel axis card veichi servo driver sd700 with motor problem unable to tune the servo motor for closed loop position control using pulse type servo amplifier control . suggest procedure for setting it up . thanks in advance Quote Link to comment Share on other sites More sharing options...
Gregs Posted January 22 Share Posted January 22 The ACC-24E3 manual has a section under the heading Pulse-and-Direction Amplifiers which applies as well to the CK3W-1414x or CK3W-1515x. Gain values for simulated loop are given as follows: It is recommended that the following servo gain values be used to close a simulated loop: · Motor[x].Servo.Kp = 40 · Motor[x].Servo.Kvfb = 0 · Motor[x].Servo.Kvff = 40 · Motor[x].Servo.Ki = 0.001 Many users will want to create a half count of deadband in the servo loop to prevent dithering between adjacent steps at rest if the command value stopped in between them. To do this, set Motor[x].BreakPosErr to 0.5 (if the motor units are equal to pulses), and Motor[x].Kbreak to 0.0. For more extensive information, see in the Power PMAC Users manual under the heading Setting Up Power PMAC for Pulse-and-Direction Control. Similar to above, it states: Parameters to Set Up Motor Servo Gains If you are using a real feedback sensor, the motor’s servo loop should be tuned just as a normal servo motor would be. This is covered in a later section of the manual. However, if you are just using the counted pulse train for feedback to create a fully electronic loop, the response is very predictable, and the tuning gains can be set directly. The following values provide a responsive and stable performance at the default servo update frequency for a motor scaled in units of pulses (counts): (Same settings as above) Quote Link to comment Share on other sites More sharing options...
Alex Anikstein Posted January 22 Share Posted January 22 Moving this to the Power PMAC forum Quote Link to comment Share on other sites More sharing options...
Recommended Posts
Join the conversation
You can post now and register later. If you have an account, sign in now to post with your account.