Unicornai Posted September 11 Share Posted September 11 I used subpro103 but i used open subprog103 close then subprog103 the occupied space is not cleared, but the size of the subprog103 data displayed on the front end has changed,what should i do about clear the disappear subprog103 size Quote Link to comment Share on other sites More sharing options...
leandro.martins Posted September 11 Share Posted September 11 (edited) If I disconnect from the hardware and connect it back after removing the subprog from buffer, then the subprogram doesn't appear in the task manager anymore. You can confirm if the subprog was removed using the command 'buffer'. Using the IDE 4.6.3.9, there is a "Refresh list" button at this version, but it has no effect on that. Edited September 11 by leandro.martins Quote Link to comment Share on other sites More sharing options...
Unicornai Posted Friday at 12:45 AM Author Share Posted Friday at 12:45 AM (edited) On 9/11/2024 at 5:27 PM, leandro.martins said: If I disconnect from the hardware and connect it back after removing the subprog from buffer, then the subprogram doesn't appear in the task manager anymore. You can confirm if the subprog was removed using the command 'buffer'. Using the IDE 4.6.3.9, there is a "Refresh list" button at this version, but it has no effect on that. thank you answer,i only want to know that how can i dispose the last subprog103 buffer,and once this situation occurs, the program will no longer free up space when it is cleared, and the final effect is that the program buffer is filled up, and subsequent programs can no longer be downloaded. My current solution is to enter $$$in the terminal. Can I ask you how I can avoid this situation or what I can do without restarting PMAC? This is my operation to clear the previous program. Could you please help me check if there are any issues open prog 6 close clear SubProg100 clear SubProg101 clear SubProg102 clear SubProg103 clear SubProg104 clear SubProg105 clear SubProg106 open subprog 100 close open subprog 101 close open subprog 102 close open subprog 103 close open subprog 104 close open subprog 105 close open subprog 106 close Edited Friday at 12:52 AM by Unicornai Quote Link to comment Share on other sites More sharing options...
leandro.martins Posted Friday at 10:13 AM Share Posted Friday at 10:13 AM I think that these both methods are redundant clean subprog 100 and open suprog 100 close What do you get from the command 'buffer' before and after the 'clear'? I might not be clear enough, but when I tried the 'clear' command had freed the memory, what could be seen by the 'buffer' command, but the task manager doesn't reflect that until I disconnect the IDE from the controller and connect it back. Quote Link to comment Share on other sites More sharing options...
Unicornai Posted 12 hours ago Author Share Posted 12 hours ago On 9/13/2024 at 6:13 PM, leandro.martins said: I think that these both methods are redundant clean subprog 100 and open suprog 100 close What do you get from the command 'buffer' before and after the 'clear'? I might not be clear enough, but when I tried the 'clear' command had freed the memory, what could be seen by the 'buffer' command, but the task manager doesn't reflect that until I disconnect the IDE from the controller and connect it back. Make sure my program has been cleared before I download it, and the memory has been freed up so that my next program can be downloaded correctly, that's all, and now I have added these clear commands, but the memory occupied by the program will not be freed, this is the question I want to ask... Quote Link to comment Share on other sites More sharing options...
Recommended Posts
Join the conversation
You can post now and register later. If you have an account, sign in now to post with your account.