Jump to content
OMRON Forums

Power PMAC Reset failed with "MacroControllerInit" on startup


RafaelFalcaro

Recommended Posts

Hi, I have three PowerPMAC BrickLV Firmware 2.6.1.0 configured in MACRO ring.

I've created a MACRO initialization PLC that executes the CMD "MacroControllerInit". This PLC is called by PowerOnMotor PLC (on startup).

When I deploy the code to the controller ($$$*** -> Build and Download All Programs -> save -> $$$), it fails the reset, and I need to reboot the controller mannually from Linux environment (or power cycle). But, after the reboot, the project loads fine, and there's no more problems on controller reset. I checked the project saved to the Power PMAC memory and the PLC in question is present.

Why the reset fail only occours in first reset after the project deploy?

Link to comment
Share on other sites

  • Replies 2
  • Created
  • Last Reply

Top Posters In This Topic

Top Posters In This Topic

Something to note:

If the project has MACRO setup changes in script header files (“.pmh”) and in the power-on PLC, conflicts with saved setup elements and the power-on PLC can sometimes happen at startup. It might be useful to have the power-on PLC with an initial timeout to avoid situations as this.

Link to comment
Share on other sites

Join the conversation

You can post now and register later. If you have an account, sign in now to post with your account.

Guest
Reply to this topic...

×   Pasted as rich text.   Paste as plain text instead

  Only 75 emoji are allowed.

×   Your link has been automatically embedded.   Display as a link instead

×   Your previous content has been restored.   Clear editor

×   You cannot paste images directly. Upload or insert images from URL.


×
×
  • Create New...