bradp Posted July 18, 2008 Share Posted July 18, 2008 In a PLC program I want to home a motor. In PMAC it was important to first set the Home Complete bit false so that it could be monitored by the PLC to know when the trigger was found. In Power PMAC I am not allowed to write to Motor[n].HomeComplete. What is the recommended method in Power PMAC to home a motor from a PLC? Link to comment Share on other sites More sharing options...
bradp Posted September 17, 2008 Author Share Posted September 17, 2008 [quote=brad] In a PLC program I want to home a motor. In PMAC it was important to first set the Home Complete bit false so that it could be monitored by the PLC to know when the trigger was found. In Power PMAC I am not allowed to write to Motor[n].HomeComplete. What is the recommended method in Power PMAC to home a motor from a PLC? [/quote] Here is a simple snippet of code that looks very good for commanding a homing search move from a PLC program, plus making sure it starts and finishes: open plc 1 ldata.Coord=1 // This must be CS motor is defined in for sync var to work ldata.Motor=1 // Necessary if want the actual home command to be motor-independent L1=ldat.Motor // So can use as index P1=0 // Starting condition P1==1 // Will occur at start of homing search move home // Acts on addressed motor (could do HOME1 if don't want addressing) while (P1==0) P2++ // Wait for move to start (P2++ for debugging only) while (Motor[L1].HomeComplete=0) P3++ // Wait for trigger to be found (P3++ for debugging only) while (Motor[L1].DesVel!=0) P4++ // Wait for post-trigger move to complete (P4++ for debugging only) close Of course depending on your philosophy, this could be made shorter or longer. The conditions could be combined into a single compound condition, and the HomeComplete condition might not be required. On the other hand, if you wanted to handle possible errors, you would need longer and more complex logic. Link to comment Share on other sites More sharing options...
Recommended Posts