bradp Posted March 30, 2009 Share Posted March 30, 2009 How do i make an FTP connection to Power PMAC?[hr] The ftp root on the powerpmac is /var/ftp. You cannot place anything there. You can only place data in the subfolders. From a Windows host you can use the Explorer and enter in the IP address as ftp://192.168.0.200 Then you will be able to explore the FTP area as any other drive. This will allow drag and drop of files to and from the PPmac From a Windows host you can also use the old DOS shell (now called CMD) and just enter the address as ftp://192.168.0.200 Then you can use the DOS commands to navigate. From a Linux host you can use the Nautilus file browser and enter in the IP address as ftp://192.168.0.200 Then you will be able to explore the FTP area as any other drive. This will allow drag and drop of files to and from the PPmac From a Linux host you can use a terminal. Here is an example of opening the FTP connection and transferring a file. root@lt-linuxhenry:/opt/eldk-4.2/debian_rootfs/opt/ppmac# ftp ftp> open 10.34.9.210 Connected to 10.34.9.210. 220 (vsFTPd 2.0.5) Name (10.34.9.210:root): anonymous 230 Login successful. Remote system type is UNIX. Using binary mode to transfer files. ftp> put /tmp/errors.txt usrflash/ local: /tmp/errors.txt remote: usrflash/ 200 PORT command successful. Consider using PASV. 553 Could not create file. ftp> put /tmp/errors.txt usrflash/test.txt local: /tmp/errors.txt remote: usrflash/test.txt 200 PORT command successful. Consider using PASV. 150 Ok to send data. 226 File receive OK. 46886 bytes sent in 0.33 secs (136.7 kB/s) ftp> Link to comment Share on other sites More sharing options...
Recommended Posts