bradp Posted March 23, 2010 Posted March 23, 2010 --- To change the nameserver do the following from telnet. 1. goto the proper directory --> cd /.readonly/etc 2. make the folder read write --> mount -o remount,rw / 3. create and or edit the file --> resolv.conf It needs to have the line nameserver {ip} example nameserver 10.10.98.7 4. make the folder read only --> mount -o remount,ro / 5. reboot the ppmac --- To change the gateway it is easiest to use the IDE. Go to tools->options and select PowerPMAC->IP Address Change Setup. Here you can change the gateway.
Recommended Posts