scott.eichhornetrema.com Posted June 8, 2010 Share Posted June 8, 2010 I'm trying to connect to my new Power PMAC via our LAN. I've assigned the PMAC a static IP. I can ping the PMAC IP and get a good response. I can connect the PMAC Suite on startup if I select the PPmac server protocol instead of Telnet. However, when opening new windows such as "motor setup" or task manager, they will not connect using either protocol. The other windows still show an online status, but new ones never connect. Any suggestions? Thanks, Scott Link to comment Share on other sites More sharing options...
scott.eichhornetrema.com Posted June 9, 2010 Author Share Posted June 9, 2010 We have gotten secure shell (port 22) to connect properly, but that isn't a protocol option for the IDE. I've made sure that port 23 (Telnet) is allowed on the LAN and I'm testing with a Windows XP system with no firewall running. Any ideas? Thanks, Scott Link to comment Share on other sites More sharing options...
hbausley Posted June 9, 2010 Share Posted June 9, 2010 Scott, I suspect you have a PowerPMAC with a video option? Telnet has a 10-20 second delay if it attempts to perform dns resolution which happens when you have a system with the video option. 1.) To remove the delay login into powerpmac using telnet. Use your favorite utility ie. Windows Hyperterminal, or add the command line telnet to Windows or download putty.exe at http://www.chiark.greenend.org.uk/~sgtatham/putty/download.html . login as root with the password deltatau then add the IP address of your PC to the PowerPMAC hosts file. For example if your PC has an IP of 10.34.9.21 issue the following commands from the linux prompt after you have logged in mount -o remount,rw / echo 10.34.9.21 IP_10_34_9_21 >> /.readonly/etc/hosts echo 10.34.9.21 IP_10_34_9_21 >> /etc/hosts mount -o remount,ro / 2.) We already automatically add 192.168.0.1 through 192.168.0.254 to the /etc/hosts file so the alternative would have been to give your PC a static IP 192.168.0.x address. 3.) We are in the process of making the default client SSH which doesn't try to perform the dns resolution before login and does not have the 20sec login delay like telnet. 4.) The Server communication option is still in test and all the controls have not been tested with it yet. [quote='scott.eichhorn@etrema.com' pid='437' dateline='1276026410'] I'm trying to connect to my new Power PMAC via our LAN. I've assigned the PMAC a static IP. I can ping the PMAC IP and get a good response. I can connect the PMAC Suite on startup if I select the PPmac server protocol instead of Telnet. However, when opening new windows such as "motor setup" or task manager, they will not connect using either protocol. The other windows still show an online status, but new ones never connect. Any suggestions? Thanks, Scott [/quote] Link to comment Share on other sites More sharing options...
scott.eichhornetrema.com Posted June 9, 2010 Author Share Posted June 9, 2010 Thanks, that worked smoothly. Now the IDE is syncing up again. Scott Link to comment Share on other sites More sharing options...
Recommended Posts