andyf Posted July 29, 2010 Posted July 29, 2010 We are looking to write a Linux driver for Ethernet communications with the Power PMAC. We would like to know if the Power PMAC Ethernet protocol is the same as that published in the Turbo PMAC2 HRM. If not, do you have any documentation covering the Power PMAC Ethernet protocol?
hbausley Posted July 30, 2010 Posted July 30, 2010 You already have a native Linux driver for the Power PMAC. It is either the ssh client or telnet client. Login using root and the default password of deltatau then type gpascii from the command prompt and our motion control engine will interpret the PowerPMAC commands. [quote='andyf' pid='583' dateline='1280425307'] We are looking to write a Linux driver for Ethernet communications with the Power PMAC. We would like to know if the Power PMAC Ethernet protocol is the same as that published in the Turbo PMAC2 HRM. If not, do you have any documentation covering the Power PMAC Ethernet protocol? [/quote] 1
Recommended Posts