Jump to content
OMRON Forums

Delta Tau Add-Ins do not show in the IDE tools menu


bradp
 Share

Recommended Posts

[b]Problem:[/b] Delta Tau Add-Ins do not show in the IDE tools menu. This means Task Manager Plot Scope Motor Setup Etc Are not shown. [b]Solution:[/b] 1. The Add-Ins are installed in the folder My Documents. If My Documents is really a network drive then the Add-Ins will not work. 2.
Link to comment
Share on other sites

  • 4 weeks later...
  • Replies 1
  • Created
  • Last Reply

Top Posters In This Topic

Top Posters In This Topic

I got an internet link to these instructions (I think from BradP originally) for a similar problem with "FogBugz" add-in, but if you replace the fogbugz add-ins for the PPMAC addins the instructions are identical. I think I got this from Brad in an email a while back: Cause: The add-in is installed on a network drive, probably because your home directory ("My Documents") is located on a server on your Intranet. Solution: Copy the add-in to a local hard drive, by following these steps: 1. Say "No" to the error message -- do not remove the add-in. 2. Exit Visual Studio. 3. Make a directory on your hard drive, for example c:\Program Files\FogBugzForVisualStudio. The name doesn't matter but it does need to be on a local hard drive, not on the intranet. 4. Find the two files that make up the add-in. They should be located in "My Documents" in a subdirectory called Visual Studio 2005\Addins. The two files are: o FogBugzForVisualStudio.AddIn o FogBugzForVisualStudio.dll 5. If the .AddIn file ends with an underscore (FogBugzForVisualStudio.AddIn_), rename the file to remove the underscore. 6. Move those two files into the directory you created. 7. Run Visual Studio 2005. 8. Choose Tools | Options 9. Go to the Environment | Add-in / Macros Security tab 10. Click Add and point to the directory where you put the add-in 11. Click OK 12. Restart Visual Studio 13. Choose Tools | Add-in Manager and check the box next to FogBugz for Visual Studio. Also check the box in the Startup column. 14. FogBugz for Visual Studio should load. More details: FogBugz for Visual Studio is a .NET assembly. When Visual Studio loads add-ins in the form of .NET assemblies over a network from the Intranet zone, it does not completely trust them. This generates a security violation.
Link to comment
Share on other sites

Guest
This topic is now closed to further replies.
 Share


×
×
  • Create New...