bradp Posted January 25, 2011 Share Posted January 25, 2011 The IDE remembers each IP address to which you connect and stores them in a drop-down box. Sometimes the addresses there were only for testing purposes and should be removed after the test is done. If this is the case the procedure to remove the IP address is: 1. Select the desired IP address from the drop-down list. 2. Right-Click on the column IPAddress which is to the right of the IP address, a pop-up menu will appear. 3. Select the menu item "Remove IPAddress from the list" [attachment=1424:name] Link to comment Share on other sites More sharing options...
michaelthompson Posted January 26, 2011 Share Posted January 26, 2011 Can we expect host names to be supported in the IDE at some point? Link to comment Share on other sites More sharing options...
bradp Posted January 26, 2011 Author Share Posted January 26, 2011 Yes. I do not think it will make the Jan 2011 release but we hope it will be in a service pack a month or so afterwards. Link to comment Share on other sites More sharing options...
Recommended Posts