Jump to content
OMRON Forums

Recommended Posts

Posted

Hi

Is there a register I can look at to determine the number of program lines remaining in a buffer running on CS1?

I am creating a custom block of data to copy over DPRAM and this is the only number I can not find a register for.

If you use background data copying it is done for you (copied to $60000) so I assume it must exist somewhere

 

Can anybody point me to it?

  • Replies 1
  • Created
  • Last Reply

Top Posters In This Topic

Popular Days

Top Posters In This Topic

Posted

There is no register for this as it is calculated by PMAC on demand. Using the “DPRAM Background Data Reporting Buffer” to get the results of the “PR” command would be the easiest method. You could also setup DPR ASCII communication and place the “PR” command in the command buffer and then set the command bit and then ‘parse’ the response from the response buffer. See the description in the Turbo PMAC User Manual for details.

 

 

Guest
This topic is now closed to further replies.

×
×
  • Create New...