andreslobo Posted August 19, 2011 Share Posted August 19, 2011 Just bought another backup board for my ancient press brakes. 1. This board is sn 8417 and it has a much larger eeprom for the firmware on the daughter board. Can I flash this with my pe win just like the other ones I have? 2. The board arrived without the metal tab that wraps around the 60 pin connector and locates it in the PC backplane. Can I buy one? If so where? Link to comment Share on other sites More sharing options...
Sina.Sattari Posted August 19, 2011 Share Posted August 19, 2011 andreslobo, Please post the part number of the base board and CPU. The part numbers usually start with a 603 or 602 number. Regards, Link to comment Share on other sites More sharing options...
andreslobo Posted August 19, 2011 Author Share Posted August 19, 2011 andreslobo, Please post the part number of the base board and CPU. The part numbers usually start with a 603 or 602 number. Regards, the main board part number is 602191-103 The daughter board is 602398-100 sn 3941 Link to comment Share on other sites More sharing options...
Sina.Sattari Posted August 19, 2011 Share Posted August 19, 2011 andreslobo, As noted in this post http://forums.deltatau.com/showthread.php?tid=65, in order to change the firmware for 602398 CPU, you have to replace the chip. Please contact Delta Tau sales channels in order to get an EEPROM chip with your desired firmware version. Regards, Link to comment Share on other sites More sharing options...
Recommended Posts