Jump to content
OMRON Forums

Driving inductive load from GeoBrick LV GPIO


wlewis
 Share

Recommended Posts

I wish to drive a small solenoid from the using the GPIO on a GeoBrick LV. Details from the manufacturer documentation follows:

 

Each valve requires 24 V DC (+10%, -15%) at 0.5 W (approximately 20 mA) to operate.

 

My concern is with another statement that they put in their documentation:

 

A point to remember in choosing or designing control circuitry is that the valves are inductors and the control electronics should be protected (by bypass diodes) against the voltage surges which will arise when the valves are switched off.

 

Is this required, or is there sufficient protection in the GeoBrick LV output circuitry to avoid the need for the bypass diodes?