daves Posted May 10, 2012 Share Posted May 10, 2012 How do I implement an early exit from a sub procedure (in a motion program)? I can't get it to work or the script parser can't handle it. I want the following: sub: MoveDOffLimit(ID, PerEU, HomeVel, &Error) local iLim; if (AxisSimulate(ID)) return; callsub sub.GetDOnLimit(ID, &iLim); if (iLim) // Code removed return; This gave error "invalid parameter number in equation : R0=ID CALLSUB 10003 iLim=R1" I thought that was a hint to move iLim... sub: MoveDOffLimit(ID, PerEU, HomeVel, &Error) if (AxisSimulate(ID)) return; local iLim; callsub sub.GetDOnLimit(ID, &iLim); if (iLim) // Code removed return; but that just gave error "invalid parameter number in equation : R0=ID CALLSUB 10001 L0=R1" so I ended up having to do sub: MoveDOffLimit(ID, PerEU, HomeVel, &Error) local iLim; if (AxisSimulate(ID) == 0) { callsub sub.GetDOnLimit(ID, &iLim); if (iLim) // Code removed } return; but this doesn't seem ideal Link to comment Share on other sites More sharing options...
Recommended Posts