Jump to content
OMRON Forums

Recommended Posts

Posted

I have troubles communicating with a Pmac2A/PC104 through Acc-2P.

I am able to program the IP address, the card replies to ping (both from Pewin32Pro2 and "dos" command) but refuses to communicate.

 

The CPU is a 80 Mhz 5CF option.

 

Since I have another identical CPU (with opt12 added) I tried with this one and.... this way it works, so it's not a fault of the ACC2P.

 

I tried resetting the card with E3 jumper with no result.

Swapping the CPUs I noticed that with the "bad" one if I plug the USB cable with the PMAC already powered windows says that the USB device could not be recognized, but if I power the device with the cable already inserted it is correctly recognized (tough it doesn't communicate through USB or ETH)

 

Any hints?

 

Both boards are new, assy 603670-109

  • Replies 1
  • Created
  • Last Reply

Top Posters In This Topic

Top Posters In This Topic

Posted
It seems that the PMAC2A/PC104 is having an hardware problem and there is nothing we can do without having the card back in Switzerland to check it.
Guest
This topic is now closed to further replies.

×
×
  • Create New...