dennisg Posted June 6, 2012 Share Posted June 6, 2012 Hello All, I am a complete newbie to this IDE and architecture. How do I load and execute a .plc file ? I think it is done from the Tools->Task Manager but it is less than obvious for me how to do that. TIA. Link to comment Share on other sites More sharing options...
Omron Forums Support Posted June 6, 2012 Share Posted June 6, 2012 In the Solution Explorer within the IDE, click on PMAC Script Language-->PLC Programs. There you can add new programs by right-clicking on PLC Programs and then selecting Add-->New Item-->Script PLC. Then, write your PLC and give it the number you want. E.g. open plc 5 // contents close To run the PLC, type the following into the terminal: enable plc 5 Link to comment Share on other sites More sharing options...
dennisg Posted June 6, 2012 Author Share Posted June 6, 2012 Thanks, I also figured out that it is RTPLC 0 and I ran it from the Task Manager. I think RTPLC means real time, I do see just a PLC in the table too. I am coming in on old code written by someone long gone. He apparently had compiled this which is why I see in in the task manager. Where can I find the info on how to do compiles on PLC code when I need to make changes to this code ? TIA. In the Solution Explorer within the IDE, click on PMAC Script Language-->PLC Programs. There you can add new programs by right-clicking on PLC Programs and then selecting Add-->New Item-->Script PLC. Then, write your PLC and give it the number you want. E.g. open plc 5 // contents close To run the PLC, type the following into the terminal: enable plc 5 Link to comment Share on other sites More sharing options...
Omron Forums Support Posted June 12, 2012 Share Posted June 12, 2012 You don't need to compile PLC code - it's interpreted. You just need to download it if you make changes. You can do this by right-clicking your solution and then clicking "Build and Download All Programs" Link to comment Share on other sites More sharing options...
dennisg Posted June 12, 2012 Author Share Posted June 12, 2012 Thanks for the reply, I eventually figured this out. Always fun learning new tools ;-) You don't need to compile PLC code - it's interpreted. You just need to download it if you make changes. You can do this by right-clicking your solution and then clicking "Build and Download All Programs" Link to comment Share on other sites More sharing options...
Recommended Posts